The Mighty Tomcat - MEOW!
Apache Tomcat/5.0.30
The Jakarta Project

Administration      
Status
Tomcat Administration
Tomcat Manager
 

Documentation      
Release Notes
Change Log
Tomcat Documentation
 

Tomcat Online      
Home Page
Bug Database
Open Bugs
Users Mailing List
Developers Mailing List
IRC
 

Examples      
JSP Examples
Servlet Examples
WebDAV capabilities
 

Miscellaneous      
Sun's Java Server Pages Site
Sun's Servlet Site
 
     

If you're seeing this page via a web browser, it means you've setup Tomcat successfully. Congratulations!

As you may have guessed by now, this is the default Tomcat home page. It can be found on the local filesystem at:

$CATALINA_HOME/webapps/ROOT/index.jsp

where "$CATALINA_HOME" is the root of the Tomcat installation directory. If you're seeing this page, and you don't think you should be, then either you're either a user who has arrived at new installation of Tomcat, or you're an administrator who hasn't got his/her setup quite right. Providing the latter is the case, please refer to the Tomcat Documentation for more detailed setup and administration information than is found in the INSTALL file.

NOTE: For security reasons, using the administration webapp is restricted to users with role "admin". The manager webapp is restricted to users with role "manager". Users are defined in $CATALINA_HOME/conf/tomcat-users.xml.

Included with this release are a host of sample Servlets and JSPs (with associated source code), extensive documentation (including the Servlet 2.4 and JSP 2.0 API JavaDoc), and an introductory guide to developing web applications.

Tomcat mailing lists are available at the Jakarta project web site:

Thanks for using Tomcat!


  Copyright © 1999-2004 Apache Software Foundation
All Rights Reserved